Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for Russian (EMEA) region.

Семейство продукта

Grounding Studies for Industrial Applications

A grounding system is one of the most important, yet neglected, segments of a critical facility’s electrical power system. Testing it is not only prudent, it is required by the National Electrical Code. Grounding studies ensure protection from low-level arcing ground faults that can destroy your switchgear in seconds and put personnel in danger. Vertiv’s grounding studies include the required tests and inspections needed to verify your system’s integrity.

Получить брошюру
Оптимальное решение для:
  • ChemicalPetrochemical excl. Oil Gas
  • Manufacturing
  • Oil and Gas
  • Power Generation
  • PowerGas Transmission and Distribution

Преимущества

More confidence in your electrical infrastructure is achieved with periodic testing to verify the integrity of the grounding system
Improved protection for systems and people occurs as electric shock can be avoided 
Fewer outages are possible as a study determines if your system adequately manages low-level arcing ground faults
Less nuisance tripping occurs when a study confirms functionality that complies with manufacturer, UL , and NEMA recommendations
Ensured compliance with safety codes and regulations occurs when studies are performed by experienced, NETA-certified technicians 

Особенности

Field acceptance testing, per NEC requirements, verifies proper installation and operation of your ground fault protection system
Bonding inspection identifies and resolves problems that can defeat ground fault protection or cause inadequate tripping
Sensor installation check eliminates false tripping that can occur with incorrect current sensor installation and wrong polarity
Relay testing ensures your system’s relay trips within manufacturer’s tolerance in order to provide adequate protection
Operations test of the overall system, including special features, verifies functionality that provides the needed protection

Найти контактные данные местного представительства

Контактные данные службы поддержки продукции

Найденные контактные данные по критерию Ohio, 43215, USA Изменения
Emergency Response for Services
+1 800 543 2378
USA
Целевые области обслуживания: Проектные услуги, Меры по оптимизации обслуживания
Geist Support - Americas (Rack PDU and Watchdog)
1777 Yolande Avenue Lincoln Nebraska USA
Целевые области обслуживания: Проектные услуги, Меры по оптимизации обслуживания, Противоаварийные мероприятия, Профилактическое обслуживание, Профилактическое обслуживание для отраслевого применения, Дистанционное обслуживание, Управление запасными частями и комплектующими деталями
Vertiv (Liebert Services)
610 Executive Campus Drive Westerville Ohio 43082 USA
Целевые области обслуживания: Проектные услуги, Меры по оптимизации обслуживания, Курсы обучения, Противоаварийные мероприятия, Профилактическое обслуживание, Профилактическое обслуживание для отраслевого применения, Дистанционное обслуживание, Управление запасными частями и комплектующими деталями
ПРОДУКТЫ И УСЛУГИ
Общая информация
РЕШЕНИЯ
Общая информация
Имя для входа партнера

Язык и регион