Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for Russian (EMEA) region.

More than a third of U.S. data center managers are using colocation for cloud services, a growing opportunity for colocation providers to meet customer needs and differentiate their services.

IT capacity is being deployed in many ways, with deployments becoming increasingly diverse and complex.Colocation providers must build and scale to support a variety of deployments.

Vertiv conducted an online survey of 226 U.S. enterprise data center managers regarding their use of colocation services and their future needs for services. Respondents indicated that future IT application deployments will become more diverse and complex and that they seek colocation providers that can quickly scale capacity when needed, provide edge connectivity and offer price transparency.

  • 65% of respondents said that their organizations are using colocation data centers or will use them over the next two years

  • 57% will increase their use of colocation in the next 12 months

  • 64% of colocation users have been using these services for less than five years

  • Improving capacity scalability is the number one reason customers move to colocation, followed by edge connectivity

View The Report

Статьи на похожие темы

Visit the Colocation Exchange Image

Темы статей

Visit the Colocation Exchange
ПРОДУКТЫ И УСЛУГИ
Общая информация
РЕШЕНИЯ
Общая информация
Имя для входа партнера

Язык и регион