Activatiestatus
Neem contact op met Vertiv Partner Support: salescloudsupport@vertivco.com
Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.
Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.
Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.
Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.
Cookies Settings
Technical Cookies
These cookies are essential to ensure the correct functioning of the website, to allow you to register/login and access reserved features, and to allow us to monitor the security of the website and improve operating performance, for example, by storing your preferences to enhance your subsequent visits.
Analytics Cookies
These cookies allow us to collect and analyze traffic and use of the website on an anonymous basis and to understand and improve how visitors use the website, including which pages and products are viewed most frequently. These cookies are not strictly necessary for the website to work but will provide you a better browsing experience.
Profiling Cookies
These cookies allow us to track your navigation of the website to create profiles of your tastes, habits, choices, etc., to send you promotional messages targeted to your preferences. Refusal of these cookies will not affect the proper functioning of the website but will prevent us from being able to send your promotional messages targeted to your preferences.
By clicking “Accept All”, you agree to the storing of cookies on your device to enhance site navigation, analyze site usage, and assist in our marketing efforts.
For more information on which cookies we use, click here.
Combining Air and Liquid: The Best Solutions for High Density Data Centers
Vertiv™ Liebert® DCD
The Vertiv Liebert® DCW chilled water-based cooling family was designed specifically for high heat density applications where the challenges of reducing energy consumption and increasing processing capabilities are the top priority for data center managers. By delivering cooling directly at the source, the DCD Rear Door Heat Exchanger provides a room-neutral environment, while the DCP Coolant Pumping Unit regulates the chilled water and ensures optimal cooling capacity for mission critical equipment.
Vertiv™ Liebert® AFC
The VertivTM Liebert® AFC is the Inverter Screw Chiller Range with Low-GWP Refrigerant from 650 to 2200 kW.
Liebert® AFC, as a result of its new low global warming potential (GWP) HFO refrigerant and inverter technology, offers a solution, aiming at significantly reducing direct and indirect CO2e emissions into the atmosphere, and limiting the carbon footprint of the data center.
Vertiv™ Liebert® PCW
The Vertiv™ Liebert® PCW is the Chilled Water Perimeter Unit from 25 to 400 kW Designed to Lead the Thermal Management Market for Chilled Water Perimeter Units to meet the demands of both raised and non-raised floor applications.
One unit and four key concepts: increasing the cooling density, maximizing the cooling continuity, setting new efficiency standards and perfectly adapting to each data centre configuration.
Liebert® PCW comes complete with the integrated Vertiv™ Liebert® iCOM™ smart control, which embeds a comprehensive algorithm library adjusting the airflow to the servers’ needs without wasting a single Watt on unnecessary cooling or air movement.
Vertiv™ Liebert® CWA
The Vertiv™ Liebert® CWA is the Chilled Water Thermal Wall Unit from 200 to 500 kW designed to rise the technology threshold of Chilled Water Air Handling Units for slab floor applications installed in the gallery side.
Liebert® CWA provides a ready-to-use Thermal Wall for data center applications. The product has been engineered to maximize the cooling density for unit footprint.
Furthermore, all the main components are factory installed, minimizing the installation costs on site.
Liquid Cooling Services
IT and Facility teams can leverage partner project services to prepare for onsite liquid cooling installation, commissioning and start-up.
Project Phases and Services include:
Navigating application design
Conducting offsite testing
Providing project management
Installing the new system
Starting up systems
Handing over the new system
Teams will also want to investigate ongoing services from equipment manufacturers to protect costly liquid cooling systems and ensure effective operations; such as conducting remote monitoring, managing fluids, performing preventive maintenance, and overseeing asset management.
The benefits of adding liquid cooling to your air-cooled facility
Liquid cooling can effectively manage up to and exceeding 120kw per rack
Learn MoreReduce total data center power consumption around 10.2%
Learn MoreMore than 15 percent improvement in total usage effectiveness (TUE)
Learn MoreTop Three Takeaways on Deploying Liquid Cooling
Here is high-level guidance any team can use to navigate the incremental addition of liquid cooling to air-cooled environments cooling infrastructure.
Vertiv Is Working Together with Leaders in the AI Industry

NVIDIA
- Vertiv is a Solution Consultant Advisor partner in the NVIDIA Partner Network (NPN).
- NVIDIA and Vertiv have been collaborating in the latest liquid cooling technologies to enable cutting-edge chips to run effectively, such as in the US government funded COOLERCHIPS program.
Intel
- Vertiv has been partnering with Intel on liquid cooled solutions for their cutting-edge Gaudi®3 AI accelerator platform.

Additional Resources
![]()
Case Study: Colovore
Colovore deploys liquid cooling solution to offer customers rack capacities up to 50kW
![]()
Video: The Evolution of Liquid Cooling
With high-density computing on the rise, liquid cooling technologies are emerging as solutions to increase data center efficiency and sustainability.
![]()
Blog: Innovating Out Loud
Cooling Tomorrow’s Data Centers through Innovation and Collaboration NVIDIA collaborated with Vertiv™ and several industry leaders from universities, startups, and other vendors to propose a cooling system that helped NVIDIA and its partners secure a $5 million grant from the US government COOLERCHIPS program.
![]()
Press Release: Vertiv™ Acquisition of CoolTera Ltd. Boosts Liquid Cooling Portfolio
This deal will strengthen Vertiv’s capabilities to support the deployment of AI at scale.
![]()
Press Release: Vertiv™ Collaborates with Intel on Liquid Cooled Solution for the Intel® Gaudi®3 AI Accelerator Platform
Intel’s next generation AI accelerators will be supported by Vertiv liquid-cooled data center infrastructure solutions to help organizations accelerate AI adoption while achieving sustainability goals.