The page you're viewing is for Korean (Korea) region.

Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.
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
Freecooling, Evaporative and Adiabatic Cooling Technologies in Data Center Applications

The traditional cooling approach considers open aisle architectures with return air temperatures to cooling units between 22-26°C and supply air temperatures to the data center between 10-14°C to be considered standard.

With the use of intelligent air distribution management to the servers, data center designers and facility managers can increase chilled water temperatures from the standard 7-12°C, to 20-26°C.

As a result of the SmartAisle cold aisle containment solution, the servers’ exact cooling and airflow needs are met, thus investing only necessary kilowatts in targeted cooling. The SmartAisle solution increases space efficiency and provides uniform and predictable temperature to all IT equipment, directly controlling cold aisle temperature and humidity.

Combined with the right chiller, such as the Liebert® HPC freecooling chiller or the Liebert AFC adiabatic freecooling chiller, the benefits are even greater:

  • Higher capacity at smaller footprint
  • Significant energy savings as a result of the freecooling usage for a significant number of hours per year
  • Low noise operation

In this paper, we will investigate the impact of using freecooling technologies with and without adiabatic and evaporative technologies in major EMEA cities.

관련 자료

PARTNERS
파트너 로그인

언어 & 지역