The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


販売代理店のECサイトを検索

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

Vertiv™ VR rack, Vertiv™ Liebert® PSI5 UPS and Vertiv™ rack PDUs expand portfolio of technologies designed to meet demands at the edge in North America

Columbus, OH [August 15, 2018] – Vertiv today introduced power and rack products to meet the unique challenges of the network edge, including the need for rapid deployment, remote monitoring and management, and end-to-end service. These products include the Vertiv™ Liebert® PSI5 uninterruptible power supply (UPS) system, the Vertiv™ VR rack, and Vertiv™ rack power distribution units (rack PDUs) with features to meet the needs of many edge sites. All products will be stocked in North America for quicker availability to help speed deployments.

The launch of these products further expands the Vertiv portfolio of edge solutions. The breadth of product and service choices is critical at the edge, where IT needs may be different from site to site and constantly evolving. A single vendor partner that can provide end-to-end infrastructure solutions and support presents strong value to companies that require edge deployment, but do not have the resources or expertise to sustain this business model.

“As we continue to monitor the evolution of the edge and further define the needs of various edge archetypes, it is clear that one of the key factors for success at the edge is flexibility,” said Angie McMillin, vice president of offering management for Vertiv in the Americas. “With this launch, we add to an edge portfolio that delivers that flexibility by giving our customers options for their edge deployments. By building a broader offering, Vertiv is helping businesses own the edge.”

The Vertiv Liebert PSI5 high performance, line-interactive UPS joins the Vertiv portfolio of rack/tower configurable UPS. This single-phase UPS system is designed for the small spaces and high rack power densities common at the edge. The 2U UPS can be remotely monitored and controlled, has multiple options to meet runtime requirements, and is available with the optional Vertiv Power Assurance Package - a lifecycle support plan that includes installation and startup, on-site service, remote oversight and a 5-year protection plan.

The Vertiv VR rack is a robust and flexible rack solution that allows for rapid deployment. Eight standard sizes are available, all featuring a frame design that delivers about 2.5 inches of additional useable depth compared to similar sized racks, for ease of installation and maintenance of critical equipment. The rack is complemented by a variety of tool-less accessories to help speed deployment and facilitate rack management.

The new Vertiv rack PDUs are available in basic and intelligent models, stocked for rapid delivery. Intelligent models can monitor input power to plus or minus 1 percent accuracy, in addition to standard readings including amps, volts, watts, kWh and power factor. Switched models are available with the ability to monitor and control input power at each outlet, hot swappable modules to allow rapid change in the field, and patented U-lock receptacles that lock any cord in place to eliminate unintentional disconnection are among other notable features. All models have the industry’s best  5 year warranty, when registered within 120 days of purchase, and may also be supported by the Vertiv Distribution Assurance Package lifecycle support, which includes startup, installation, maintenance, repair, emergency response and other features.

To learn more about other Vertiv offerings, please visit www.Vertiv.com.

About Vertiv

Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the Chloride®, Liebert®, NetSure™ and Trellis™ brands. For more information, visit Vertiv.com.

Contact:
Vince McMorrow
614-383-1622
Vince.McMorrow@Fahlgren.com

PARTNERS
概要
Partner Login

言語と地域