The page you're viewing is for Italian (EMEA) region.

Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

The page you're viewing is for Italian (EMEA) region.

Condition-Based Maintenance services: Data-driven maintenance model

settembre 16, 2024

The main goal of a maintenance strategy is to prevent costly unplanned outages caused by equipment failures. However, considering the increased growth, resource requirements, and challenges that data centers have been facing, the current time-based delivery and reactive maintenance program that operators have in place seem inapplicable to the changing demands of the future.

Through advanced analytical methods, including artificial intelligence and machine learning (AI/ML), Condition-Based Maintenance (CBM) Services can generate precise health scores indicative of potential failures at the component-, subassembly-, unit-, or system-level. Using data from machines connected to the Vertiv™ Cloud, this proactive monitoring allows for the swift detection of equipment anomalies and estimation of useful remaining life, resulting in health incident reports, optimal servicing schedules, and service notifications ahead of potential failures that guide operational teams and engineers. This strategic approach enables data center operators to:

  • Integrate equipment and monitoring tools: Advanced monitoring tools are integrated with algorithm outputs. These tools notify operational and Vertiv teams when assets or components exhibit anomalous behaviors that warrant service considerations and are validated accordingly.
  • Improve and streamline data center management: This approach minimizes unexpected downtimes, improves service budget forecasting, and streamlines field service management. By calculating equipment conditions using correlated equipment data, non-emergency maintenance visits and component replacements can be scheduled based on actual data instead of arbitrary timelines.
  • Collaborate on a continuous basis: The algorithms are developed in collaboration with subject matter experts (SMEs) and component manufacturers from design to deployment. Using advanced AI/ML techniques, these algorithms are constantly improved, data undergoes rigorous curation and transformation, and systems maintain peak operational performance.

Optimize your data center and industrial facility maintenance with Vertiv™ Condition-Based Maintenance Services. Download the white paper to learn how Vertiv can transform the data industry’s maintenance strategy.

Condition-Based Maintenance Services address data center challenges

Download whitepaper

Articoli correlati

AI Hub di Vertiv Image

Campagna

AI Hub di Vertiv
PARTNER
Presentazione
Login dei partner

Lingua & Ubicazione