Sorry, this page isn't available for your location.

The page you're viewing is for Italian (EMEA) region.

Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

Sorry, this page isn't available for your location.

The page you're viewing is for Italian (EMEA) region.

‘Data Centres are the IoT Environment’s Workhorse’:
Vertiv Shares Expertise at IoT West Africa Conference and Exhibition

ottobre 12, 2023

Vertiv Supports Annual Event as Silver Sponsor

Lagos, Nigeria [October 12, 2023] – “When it comes to IoT, the data centre is essentially the workhorse of this environment - effectively, we are breaking the data centre space down into smaller pieces to bring the processing closer to the consumer, which is how core data centres and edge computing fit into the IoT space.” This is according to Jon Abbott, telecom strategic clients director for EMEA at Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, while speaking at the IoT West Africa Conference and Exhibition. 

During the exhibition, which was held in Lagos, Nigeria earlier this year, Abbott presented to delegates on the topic of ‘The Importance of both Core and Edge Data Centre Rollout in Supporting the Development of IoT’, and also shared his views, together with other presenters, during the panel discussion on ‘Advancing Data Centres’ Critical Infrastructures’. 

MarketResearch.com notes that the growing transition from traditional to digital ecosystems across industries is creating a huge demand for connectivity, resulting in the growing demand for Internet of Things (IoT) based solutions, adding that: “the continuous improvements in cloud infrastructure and reduced data service costs are fueling the digitalisation of industrial processes.” 

In particular, this industry intelligence provider states that the Middle East and Africa IoT market is projected to grow from US$ 33.01 billion in 2022, to US$ 138.27 billion by 2028 - an anticipated increase of over US$ 100 billion in approximately five years. 

Speaking briefly on the pervasive and trending topic of artificial intelligence (AI), which complements IoT, Abbott noted: “While data is the new oil, it has to be mined by an engine that can both understand what it’s looking at, and be capable of managing millions of pieces of incremental data. And this is really what the future of AI and machine learning is.” 

Panel discussion: Advancing data centres’ critical infrastructures 

With net-zero and ESG targets on clients’ minds, there is more pressure than ever for data centres to use less energy and become more efficient and environmentally friendly. This makes it critical for project stakeholders to work together to identify creative solutions to increase productivity and satisfy demands for speedy deployment, while also navigating the challenges brought by the market. 

During the panel discussion, Abbott and his fellow panellists discussed the advancement of data centre critical infrastructure and examined its major challenges. On IoT,  Abbott noted: “IoT brings the ability to pick up billions of pieces of information, collate and process them for the advantage of efficiency, learning or enhancement in some way. 5G is necessary to connect the sheer volume of IoT devices.” 

In this regard, he explained that the growing number of subsea cables at designated coastal venues are integral for the growth of data, powering the internet and with it the IoT. 

“All parties involved in sea cable landfalls should function as an ecosystem to best support data center deployments.,” he said, “through regulation, planning, commissioning, construction and so forth, to maximise the successful growth of data and bring its required infrastructure to the continent.” 

On infrastructure challenges and digitilisation regulation within Africa, Abbott noted: “Regulation should not hold growth on a leash, otherwise it risks being left behind. At the same time, growth should be sustainable. I would advise regulators to engage more stakeholders in order to  best support the growth of data centres and other digital infrastructure. This type of thinking and engagement is integral to assisting countries in their digitalisation journeys,” he concluded.

Exhibition attendees enjoy Vertiv’s VR applications 

Visitors to the IoT West Africa conference and exhibition were able to connect with Vertiv experts at its exhibition stand, as well as enjoy a Virtual Reality (VR) tour at the booth, allowing them to experience Vertiv’s data centres in a virtual manner, as well as enter a raffle to win Vertiv™ desktop UPS systems during the three days of the conference. 

Vertiv offers customers a VR experience of its large-scale modular data centres, as well as its power and thermal management solutions. Through the power of virtual reality, visitors were able to experience Vertiv's capabilities, by wearing a headset and using hand controllers to navigate the VR environment, interact with equipment, and watch animations that demonstrate a product’s value and key features. 

The exhibition aimed to highlight game-changing technologies, providing a platform for delegates to experience and explore the latest developments and best practices. Today’s advanced solutions will assist businesses in their digital transformation, with live demonstrations at the exhibition - such as Vertiv’s VR applications - showcasing some of the latest benefits of digitalisation. 

For more information on Vertiv’s edge computing solutions, vist the Vertiv website.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com. 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

CONTACT

Jacqui Gradwell
T + 27 63 608 2339
E Jacqui.Gradwell@vertiv.com

PARTNER
Login dei partner

Lingua & Ubicazione