Sorry, this page isn't available for your location.

The page you're viewing is for Italian (EMEA) region.

Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.

Ulteriori informazioni

Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.

Trova un reseller

Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.


Trova un reseller online

Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.



Contatta un esperto di Vertiv

Sorry, this page isn't available for your location.

The page you're viewing is for Italian (EMEA) region.

Vertiv Case Study: EPFL – École Polytechnique Fédérale de Lausanne

febbraio 12, 2019

The École polytechnique fédérale de Lausanne (EPFL) is – in addition to the many traditional universities and universities of applied sciences controlled by the cantons – one of the two Federal Institutes of Technology in Switzerland and is headquartered in Lausanne.

Since its foundation in 1969, it has become one of the best-known institutions for science and technology in Europe.

Like its sister institute in Zurich, the “ETHZ”, it has three main goals: education, research and technology transfer. Over 14,000 lecturers, researchers and students work, teach and conduct research on the main campus.

Background

To ensure the many different innovative and future-oriented projects being carried out by researchers and students are supported with the appropriate IT equipment, the EPFL has an IT and Building Infrastructure teams made up of around 200 employees. Aristide Boisseau, Head of the Datacenter Operations team, plays a particularly important role. Together with his team, he acts as the interface between the two domains, ensuring a regular exchange of information and smooth processes.

High-performance computers are predominantly used at the EPFL to provide the capacity required for scientific calculations. While the EPFL’s budget for new high performance computers has remained the same over recent years, providers have nevertheless increased the capacity of their products in the data center. As a result, the power density per square meter has risen and the existing ventilation cooling systems have not been able to keep pace with this growth. A new, intelligent solution  capable of adequately cooling the 8-point grid systems was therefore required.

Case Summary
Location:

Switzerland

Vertiv Solutions:
  • Consulting on equipment for a new IT center
  • Liebert Smart Rack PDU MPX
  • Knürr DCD35 air-water cooling doors
Results:
  • Improvement of the power usage effectiveness (PUE) value from 2 to 1.06
  • Space saving of 30% to 50%
  • Reduction of CAPEX and OPEX
Download the Case Study

Articoli correlati

Amadeus Image

Case Study

Amadeus
PARTNER
Presentazione
Login dei partner

Lingua & Ubicazione