The page you're viewing is for English (LATAM) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

Vertiv expands its global liquid cooling portfolio with the announcement of two new high-capacity coolant distribution units to support AI applications  

November 19, 2024

Vertiv™ CoolChip CDU liquid-to-liquid and liquid-to-air solutions support hyperscale, colocation and enterprise applications 

COLUMBUS, Ohio [November 19, 2024] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced a significant expansion of its liquid cooling product portfolio with the introduction of two new Vertiv™ CoolChip CDU (coolant distribution unit) systems. These systems enable modular, cost-effective liquid cooling deployments in data centers, making it possible to operate high-density computing for AI alongside traditional air-cooled racks. The new CDUs are on display at the Vertiv booth at SC24, the international conference for high performance computing, networking and storage, from November 19 - 22.  

The Vertiv CoolChip CDU family delivers much-needed flexibility to data centers and colocation providers, with capability for fast, modular growth and the ability to support multiple high-density racks from a single CDU, supporting the increasing demand for AI deployments.  Along with these new systems, Vertiv has a broad suite of global service offerings to support the deployment of liquid cooled infrastructure, ranging from solution design to installation to on-going lifecycle and fluid management.  

“The AI-focused data center necessitates advanced cooling technologies,” said John Niemann, senior vice president of the thermal business unit at Vertiv. “Vertiv's expanded liquid-cooled solutions support the densification of the data center we are seeing as a result of AI. Our liquid cooling portfolio, complemented by our full solution of air cooling, heat rejection, and re-use solutions and global services capability, enables both new and existing data centers to seamlessly introduce liquid cooling as part of the overall hybrid cooling solution to make AI deployments easier, faster and more cost-effective for customers.”  

The Vertiv™ CoolChip CDU 2300kW model is a liquid-to-liquid system that offers the most compact footprint in its capacity range, with the smaller cabinet enabling it to be placed in the row or in a mechanical gallery outside of the data center whitespace. Offering 2.3 MW of cooling capacity, this design caters to hyperscalers and colocation providers looking to deploy large scale liquid cooling solutions at the highest density. This solution has the industry’s highest CDU capacity per square foot, enabling operators to reduce cost and footprint by deploying fewer CDUs.   

The Vertiv™ CoolChip CDU 350kW model is a liquid-to-air solution that offers direct-to-chip liquid cooling support with air-based heat rejection, enabling it to easily retrofit into existing facilities and to deploy liquid cooling for direct-to-chip applications without a facility chilled water system.   

Both Vertiv CoolChip CDU systems can distribute coolant directly to liquid cooled chips and rear-door heat exchangers. Controls allow for fluctuating temperature and flow to match varying application demands. The systems leverage unit-to-unit communication for system-level control; redundant power feeds, pumps and filters for improved cooling availability; remote temperature, humidity and leak detection sensors; and integrated controls that enable remote monitoring and management.  

For more information on the thermal management portfolio or other Vertiv solutions for modern data centers, visit Vertiv.com.  

About Vertiv 

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com. 

Forward-Looking Statements 

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

CONTACT 

Brianna Rabe - Ruder Finn
E brianna.rabe@ruderfinn.com

Related Articles

PARTNERS
Partner Login

Language & Location