Sorry, this page isn't available for your location.

The page you're viewing is for English (LATAM) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (LATAM) region.

Vertiv Launches Remotely-Managed, Prefabricated Edge Data Center Infrastructure Solution in Latin America

December 05, 2022

The modular Vertiv™ SmartRow™ 2 row-based system is factory-configured and tested and quickly deployed to support mission-critical operations at the network edge

São Paulo, Brasil [December 05, 2022] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, launched today in Latin America the Vertiv™ SmartRow™ 2, an upgrade to its portfolio of prefabricated modular data center solutions for edge computing applications. This micro data center provides complete infrastructure for rack-based IT equipment, including servers and routers. SmartRow 2 is available now through Vertiv representatives and channel partners throughout Latin America.

The SmartRow™ 2 consists of a row of IT racks pre-configured and tested at Vertiv’s factory, and includes solutions for power distribution, uninterruptible power supply (UPS), batteries, cooling and mechanical support. With a plug-and-play physical infrastructure and logic, it accelerates the solution deployment process, and is ideal for installation in businesses of all sizes and all market verticals.

Alexandre Magno Alves, IMS offering manager at Vertiv LATAM explains that the Vertiv SmartRow 2 is an evolution of the previous modular data center solution, Vertiv™ SmartRow™ BR. SmartRow™ 2 offers additional intelligent resources, which allow more efficient management of edge IT applications by delivering precision controls for the complete environment.

In addition, Magno Alves emphasizes that being a standardized solution, a trend in the data center industry, the SmartRow 2 enables faster deployment, efficient operation, and a shorter learning curve compared to traditional data center builds. “This is not just a simple upgrade to the previous generation of products, the SmartRow 2 actually offers users a more compact, reliable, secure and convenient technology room experience,” said the executive.

According to Magno Alves, 5G rollouts and the exponential increase in data traffic will result in edge computing supporting users and emerging technologies through distributed IT infrastructure. “In such a model, storage and computing are brought closer to the users and devices. This requires the edge of the network to be smarter, simpler, and self-sufficient. This is exactly what the Vertiv SmartRow 2 delivers to the Latin American market.”

In addition to an embedded IT management solution, the Vertiv SmartRow 2 offers a smart lighting system that alerts on-site IT managers to problems such as out-of-range humidity, high temperature, and other conditions that may compromise the network.

Thanks to the Vertiv SmartRow 2 IT management system, it is possible to:

  • Remotely monitor and manage infrastructure devices (UPS, HVAC, sensors, etc.) and IT devices (server, router, etc.) through a single platform.
  • Enable access to the servers’ service processors (IPMI 2.0 protocol) for consulting relevant information, as well as accessto the execution commands.
  • Enable management of IT assets through serial connection.
  • Local view through an embedded HMI display and verification of remote system integrity via IP-based webpage.
  • Receive alarm notifications by e-mail or SMS, and download the activity log and alarm history for further reporting.

For more information about Vertiv™ SmartRow™ 2, please visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Tatiana Fonseca
Everton Santos
T +55 11 9-99563188
T +55 11 9-85419799
E gad@gadcom.com.br

Partner Login

Language & Location