Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Vertiv Launches New Energy Efficient and Space-Saving Power Back-up Solutions for Edge and Mid-Size Data Centers

July 05, 2022

Vertiv™ Liebert® ITA2 and Vertiv™ Liebert® EXM2 uninterruptible power supply (UPS) systems were among multiple solutions that were unveiled to customers at this year’s Vertiv Xpress Power Drive, the company’s annual city-specific partner roadshow

Mumbai, India [June 06, 2022] –Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, Vertiv launched a range of uninterruptible power supply (UPS) solutions – including Vertiv™ Liebert® ITA2 – 30 kVA, Vertiv™ Liebert® EXM2, during this year’s Vertiv Xpress Power Drive, a roadshow that showcases the company’s complete stack of critical infrastructure solutions to its end users across India. This multi-city initiative engages customers as well as partners through unique collaboration programs and works towards collectively growing the partner’s business.

The full range of power products that have been launched so far include:

  • Liebert ITA2 – 30 kVA offers best-in-class energy efficiency of up to 96.3% over a wide range of load conditions, resulting in significant operational cost savings. The Liebert ITA2 30 kVA integrated Smart Sleep technology in ECO mode provides a superlative energy efficiency of up to 99%. This rack/tower convertible UPS is ideally suited for edge and small computer room applications.
  • Liebert EXM2 100-250 kVA offers high energy efficiency in the midsize UPS range, with up to 98.8% rating in dynamic online mode and 97% in double conversion mode. It is also compatible with lithium-ion battery configurations and adapts to two-wire DC bus connection settings. The Liebert EXM2 can be deployed in an in-row, room or against the wall configuration which saves space in the facility.
  • Vertiv™ Liebert® GXT MT + CX4 1K SB systems are true double conversion online UPS systems designed to provide with a capacity of 1 kVA with inbuilt battery. The unit features total isolation of the load from the mains - isolating input and output sections, and makes the systems ideal for work from home / data networks / small data centers / Voice over Internet Protocol (VOIP) applications.
  • Vertiv™ Liebert® ITON 1000VA is an economical line-interactive UPS that offers full-featured power protection for home or small office computers and electronic equipment. Its unique features and extraordinary performance are not normally found in products in the range.
  • Vertiv™ Liebert® S600 10 and 20kVA are fully-digital, highly reliable, double conversion UPS solutions that deliver clean and consistent power. This highly efficient solution is ideal for IT racks, network closets, automation control systems, and precision instruments to small-sized control rooms, among other edge applications.

This year’s Vertiv Xpress Power Drive has covered 15 events so far in cities such as Agra, Delhi, Mumbai, Pune, and Goa between March and May 2022. It has been attended by  more than 1,000 partners and customers across all verticals and domains.

The partnership of Vertiv with National Value-Added Distributor Technobind was announced through this campaign, in cities including Delhi, Mumbai & Pune. This helped in bringing in regional distributors like Cache Technologies in Pune and Radiant Technologies in Delhi to address the IT reseller markets. Vertiv Xpress Power Drive visited several locations across the country along with partners and national distributors for live demonstrations of Vertiv’s offerings through day trainings to sales personnel of partners, followed by an evening seminar. Sonepar, an enterprise business partner in the AC power and thermal business, partnered with Vertiv earlier this year, and this was announced to its power customers and consultants at the Delhi leg of the event.

“We’re thrilled to have launched our robust power back-up performers at this year’s Vertiv Xpress Power Drive, giving customers visibility to innovative solutions right at their doorstep The increased focus on digital transformation and hybrid work over the past two years has heightend the need for enterprises to have  power back-up solutions to enable business continuity,” said Pradeep S., director, AC power sales, Vertiv India.

Vertiv Xpress.png

For more information on Vertiv and its complete portfolio of digital infrastructure and continuity solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT

Ipshita Balu

T +91 95901 11798

E ipshita.balu@archetype.co

PRODUCTS & SERVICES
PARTNERS
Overview
Partner Login

Language & Location