Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Vertiv Introduces New, Compact Cooling Solution for Edge Applications in India

September 22, 2022

Vertiv™ Liebert® SRC-G thermal management solution delivers availability and efficiency to small critical infrastructure with ‘zero’ indoor footprint

Mumbai, India [September 21, 2022] Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, has introduced the new thermal management solution Vertiv™ Liebert® SRC-G for the edge of the network in India. The new solution delivers high uptime and efficiency to small critical infrastructure, while using ‘zero’ indoor footprint. Liebert SRC-G is available now in India.

The wall-mounted Liebert® SRC-G is available in capacities from 3 kW to 11 kW, occupying no ‘white space,’ and providing year-round cooling to IT equipment. The CE-certified Liebert SRC -G series can support sensible load operation year-round. It is equipped with energy-efficient technologies, including EC fans, R410A refrigerant, and rotary or scroll compressors. The Liebert SRC-G also features an advanced controller, including remote monitoring capabilities for added intelligence when managing edge IT locations.

“Vertiv understands the growing complexities of managing computing at the edge of the network,” said Andy Liu, director for integrated rack solutions at Vertiv in Asia. “Availability, efficiency and agility are vital to our customers, and our new offerings meet these requirements, with a high-efficiency room cooling system for small IT spaces. In addition, the efficiency features can help to support our customers’ sustainability strategies in the data center space.”

The Liebert SRC-G can sustain an outdoor temperature of up to 48 degrees Celsius, comes with a hydrophilic coated coil, and a high-efficiency EC fan with high airflow of over 255 CMH/kW. It has an advanced monitoring and control system specifically designed for technology room applications, a self-diagnostic feature which assists the servicing/maintenance process and drastically reduces response time.

“With rising global warming concerns, our world is experiencing higher temperatures than before, with data center and IT infrastructure sites being no exception. As a result, equipping  small technological rooms -  such as UPS & battery rooms, IT rooms, control rooms, VFD rooms, electrical rooms and ATMs - with thermal management solutions is crucial, especially in countries with a tropical climate like India”, said Liu. “As leaders in flexible, customizable solutions, we at Vertiv continue to adapt and innovate our solutions portfolio to keep up with the changing business and environmental

For more information on the Vertiv Liebert SRC-G, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT

Ipshita Balu
T +91 95901 11798
E ipshita.balu@archetype.co

PRODUCTS & SERVICES
PARTNERS
Overview
Partner Login

Language & Location