Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Vertiv, Conapto, and Fever Energy Join Forces to Introduce Dynamic Grid Support in Sweden

Enhancing sustainability, adding capacity and contributing to a more stable grid

March 12, 2024

London, UK [March 12, 2024] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, alongside Conapto, a leading Swedish colocation provider, and Fever Energy, a key player in grid support solutions, today announced the introduction of Dynamic Grid Support in Conapto’s operations. Harnessing power from Vertiv™ Liebert® EXL S1, an innovative Uninterruptible Power Supply (UPS) system which provides an integrated solution for critical power protection and grid support capabilities, this groundbreaking initiative aims to enhance sustainability through maximum energy efficiency of the UPS and reduced CO2 emissions through use of alternative energy sources. 

As digitalisation continues to accelerate the growth of Sweden's digital infrastructure, the demand for stable, reliable and sustainable power sources has surged. Recognising this need, Vertiv, Conapto and Fever Energy have come together to give data centres the opportunity to play an active role in stabilising the grid while unlocking new revenue streams. 

Through the innovative Dynamic Grid Support feature of the UPS, Conapto can actively contribute to grid stability by participating in fast frequency response (FFR) and frequency containment reserve demand (FCR-D). Vertiv’s solution optimises UPS capacity and employs lithium-ion battery storage, enabling power support during peak utility demand, without significant infrastructure changes. By providing static and dynamic frequency regulation, along with demand management capabilities, the UPS helps grid stability and efficient resource utilisation, supporting the integration of alternative sources, such as wind, water and solar, in the energy ecosystem. 

Conapto has selected Vertiv™ Liebert® EXL S1 UPS system, based on its ability to reduce energy consumption compared to less energy efficient alternatives. This innovative solution, supported with lithium-ion battery technology, provides high capacity in a compact footprint, allowing data centres to maximise the number of racks and servers and also enables operating efficiency up to 99%. 

The joint initiative will fall into two key phases. First, existing Conapto installations acquired in 2022 are now being optimised for grid support, with UPS units tailored for end users to seamlessly integrate into the system. Next, the same solution is currently being implemented at Conapto’s Stockholm 4 South locations, enhancing grid support capacity and resilience. 

Karsten Winther, president for Vertiv in Europe, Middle East and Africa, says: "The collaboration between Vertiv, Conapto and Fever Energy represents a significant milestone in the data centre industry, and builds on our own 15 year partnership with Conapto. With the introduction of Dynamic Grid Support, we are empowering Conapto to not only enhance operational efficiency in its data centres, but also contribute to grid stability, and sustainability when paired with energy alternatives, marking a significant step forward in the evolution of critical digital infrastructure." 

Stefan Nilsson, Chief Commercial Officer at Conapto, says: "In line with Conapto's commitment to sustainability and societal contribution, we believe that data centres should not only consume energy but also play an active role in supporting the grid. By introducing Dynamic Grid Support, we can help reduce Co2 emissions by enabling more renewables to be added to the energy mix. We can also generate new capacity for our customers and deploy it much faster. Our partnership with Vertiv and Fever Energy is testament to this ethos as we work towards creating a more resilient and sustainable digital infrastructure for Sweden and beyond." 

For more information about the project, read the case study at this link. To learn more about Vertv’s portfolio and Dynamic Grid Support, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com. 

About Conapto

Conapto offers scalable, secure and sustainable data centre colocation as well as the cloud connectivity needed for companies and managed service providers to produce and deliver digital services in a hybrid IT-environment.

With Conapto’s four climate responsible data centres in Stockholm, Sweden, the company can meet the growing data capacity needs of international technology companies given the rise of compute loads with trends like Artificial Intelligence, Edge Computing and Blockchain. For further details and to stay update with the latest news from Conapto, visit www.conapto.com. 

About Fever Energy

Fever is a power technology company with a mission to transform energy assets and the power grid with software. By bringing the most advanced technology and machine learning capabilities to the power industry, Fever is changing how energy assets are utilised, powered, secured and monetised. Read more www.fever.energy

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

CONTACT

Susanna Collins
T +44 (0)7872 558593
E susanna.collins@apodpr.co.uk

PARTNERS
Overview
Partner Login

Language & Location