The page you're viewing is for English (China) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (China) region.

Gulf Data Hub Features Energy-Efficient Solutions to Enable Effective Data Center Builds

2024年7月11日

Background: 

Gulf Data Hub (GDH) is a top-tier provider of colocation services and purpose-built data centers adhering to international standards, specializing in disaster recovery, cloud solutions, software as a service (SaaS), and infrastructure as a service (IaaS).  

Vertiv’s journey with GDH started with the inauguration of the company’s data center in Dubai Silicon Oasis (DSO), boasting a capacity of 4 megawatts (MW). Presently, GDH operates six data centers within DSO, with three of them boasting a capacity of 16 MW each.  

The partnership between GDH and Vertiv spans eight years and encompasses numerous successfully executed projects.  

Results:  

The GDH data center will now be able to operate with high efficiency even in scenarios with low loads thanks to the Liebert EXL S1 UPS. With its Dynamic Online Mode and its efficiency up to 99%, it can fully support efficient data center principles while promoting lower power usage effectiveness (PUE).   

Using efficient, reliable UPS and cooling products, Vertiv produced a suitable solution for both GDH and end users who receive colocation services in the data center. 

Case Summary
Location:​

Dubai Silicon Oasis, Abu Dhabi - UAE   

Critical Need:

Balancing the ambitious architectural vision with strict budgetary constraints and achieving low-carbon energy generation while maintaining an optimal research environment. 

Vertiv Solution:
  • Vertiv™ Liebert® EXL S1 UPS 
  • Vertiv™ Liebert® CWA 

DOWNLOAD THE CASE STUDY

Related Articles

Language & Location