The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Lithium-Ion Battery Backup

Back IT Up

Lithium-Ion UPS battery backup systems are designed to provide twice the life expectancy of traditional VRLA batteries. Through fewer battery replacements, ability to withstand higher temperatures, and quick recharge cycles, these systems are ideal for protecting your critical infrastructure in edge or distributed IT environments.

Vertiv™ Liebert® Power-UPS Lithium

  • Cost-effective, high-performance, and long-lasting UPS
  • Use for: computers, workstations, retail point-of-sale (POS) equipment, wireless networks and routers, surveillance systems and other electronics

Buy now

 

 Now Available! 

 Vertiv™ Liebert® GXT5 1-3kVA Lithium-Ion UPS 

Your UPS Solution with Less Pollution

800x450-vertiv_gxt5li-5-10kva-6000mvrt3uxln.png"

 
Now Available! 

 Vertiv™ Liebert® GXT5 5-10 Lithium-Ion UPS 

Size Matters

800x450-vertiv_gxt5li-5-10kva-8000-10kmvrt4uxln.png

vertiv-liebertgxt5lio-5-10kva-vs-topcompetitors-graphic-en-na-368257-web_368258_0.png

Now Available!

Vertiv™ Liebert® ITA2 UPS

Featuring Optional Lithium-Ion Battery Cabinets

View Product

What is a Lithium-Ion Battery Backup UPS?

Uninterruptible power supply, or UPS, is a device that provides power backup to IT equipment when power completely fails or drops low enough. Some types of uninterruptible power supply provide just enough time for a computer to save what the user is doing and power down while some can provide electricity for over an hour.

Traditional UPS are manufactured with lead-acid (or VRLA) batteries. Lithium-Ion battery technology has only been around since the 1980’s. It has only been in the past two decades that the technology has been applied to uninterruptible power supply. Luckily the technology has improved enough to allow smaller businesses and IT solutions organizations to implement in everyday applications.

Industries Using Lithium-ion UPS

800x600-314736_314737_0.jpg

Retail Edge deployments are an ideal fit for Lithium-Ion UPS technology. Many large retailers are incorporating these systems into individual store locations across the country where they have increased digital needs and require reliable backup in case of an outage, and don’t have to support the maintenance that is required with traditional VRLA systems.

  • Remote retail sites
  • Warehouses and distribution

Dealing with tight spaces? Check out this information that can help

800x600-563876979-Digital-System-Education_314462_0.jpg

With the increased requirements of education to rely on technology for remote learning, schools need to ensure their systems stay up and running. Many schools are seeing the benefit of lithium-ion UPS systems in their deployments due to the total cost of ownership and reduction of maintenance with each unit.

  • K-12 Schools
  • Higher Education

Manufacturing-CH01_800x600_315238_0.png

Manufacturing floors are continuing to further advance their technologies, and the IT to support the production lines needs to be close to the equipment it is supporting. Oftentimes, this results in IT infrastructure being put in places that weren’t traditionally designed for it. Manufacturers are continuing to adopt Lithium-ion UPS systems because they can withstand higher temperatures without degrading the battery.

  • Manufacturing floors
  • IT rooms at a manufacturer

800x600-healthcare-laboratory-dark-1050311748_264480_0.jpg

From hospitals to local and remote offices, healthcare IT teams are being asked to support more demand than ever on their networks. The industry is turning to lithium-ion UPS systems to support the need for added runtime, reduction of maintenance, and overall efficiencies.

  • Private offices
  • Hospital IT rooms

Dealing with tight spaces? Check out this information that can help

Lithium-Ion Battery Backup UPS Advantages

Lower Total Cost of Ownership (TCO)

Taking into consideration the initial investment of a VRLA system in addition to the battery replacements and services that aren’t needed with lithium-ion UPS, you are able to reduce your total cost of ownership of your UPS system by 50%.

Longer Life and Runtime

The life expectancy of a Lithium-Ion UPS is 8-10 years, which is 4x longer than comparable VRLA systems. When the Lithium-ion battery needs a recharge, it can be complete in less than four hours.

 

 

Heat Resiliency

In instances where your racks are exposed to higher temperatures, such as manufacturing floors, lithium-ion batteries are a great option. These UPS systems can withstand higher temperatures without degrading compared to VRLA batteries.

Efficiency

For a much better performance, lithium-ion batteries are 40% to 60% lighter than VRLA counterparts. On top of being lighter, they are 40% smaller too. This makes lithium painless to install, easier to maintain, and significantly more flexible. Also, while typical lead acid batteries take 12 hours to charge to 90% full runtime capacity, lithium-ion only requires 2 to 4 hours.

 

Interested in learning more?

In this webinar, Vertiv discusses the different types of Lithium-Ion UPS and how they compare to lead acid batteries, answer questions around Lithium-ion battery backup safety and evaluating total cost of ownership (TCO) of lithium-ion UPS equipment.

Calculate How Much Lithium-Ion Will Save You

Utilize our Total Cost of Ownership (TCO) Calculator to find your savings.

 

In the example below, you would see the following savings when purchasing a Lithium-Ion UPS.

18% Savings Versus VRLA

2200 VA over 5 Years
Standard VRLA UPS purchase of $960
1 Battery Replacement
Estimated Cost per Battery of $315
Estimated Cost per Battery Replacement $200

Find my savings

LIO-TCO-Screen-03_328479_0.jpg

UPS SELECTOR

Quickly Locate the PSI5 Lithium-Ion UPS For Your Business

Search and purchase directly from one of our reseller partners.

 

Buy now

The Backup for Your Backup

Services and Warranties for PSI5 Lithium-ion UPS products.

 

Warranty

The Vertiv Liebert PSI5 Lithium-Ion UPS is backed with a 5 year standard warranty on the UPS and the battery.

Learn more

 

Services

Let us manage your equipment with the Power Assurance Package. This all-inclusive package includes everything from power startup to emergency services.
Learn more

Upgrade VRLA to Lithium-Ion Battery Backup

With the Vertiv Trade-In Program

If you have been considering upgrading your legacy UPS systems in order to take advantage of the higher reliability, capacity, and energy efficiency of today’s newest UPS technologies, now is the time. With the Vertiv Trade-In program, you can trade in almost any aging single-phase UPS unit*—Vertiv or a competitor’s brand—and choose to upgrade to a new Vertiv GXT or Liebert PSI UPS system, including the Vertiv Liebert PSI5 Lithium-Ion UPS.

Learn more

eligible-for-vertiv-trade-in-program-600x600

We’ve Got This. Tell Us About Your Edge

Tell us about your project, and we will work with you to understand your requirements and connect you with the right IT infrastructure for your edge.

First Name *
Last Name *
Email Address *
Company *
Country *
Zip Code *
Comment
Privacy Notice Consent

Having received and read this privacy notice on personal data processing (provided in accordance with Article 13 of EU Regulation 679/2016), I consent to:

  The processing of my personal data for marketing purposes, including staying informed by email about industry trends, events, offers and product launches.



 

 

Thank you for your submission!

What's Your Edge?
Partner Login

Language & Location