The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Vertiv Announces Upgrade to Industry’s Most Popular Rackmount On-line UPS for Critical Network and Edge Applications

June 10, 2019

Vertiv™ Liebert® GXT5 boosts power and efficiency, enhancing the small space segment of the premium UPS channel portfolio in North America

Columbus, Ohio [June 10, 2019] – Vertiv today introduced the Vertiv™ Liebert® GXT5, a technology update to the popular family of rackmount, on-line uninterruptible power supply (UPS) systems. The Liebert GXT5 is designed to ensure availability in today’s increasingly mission critical small IT environments and edge locations that enable important emerging applications such as 5G, virtual and augmented reality, and the Internet of Things. Vertiv made the announcement at Cisco Live, an industry event for Cisco technology users and partners.

The Liebert GXT5 is the latest addition to the Vertiv channel product portfolio in North America. It has a power factor of up to 1.0 on select models, providing more real power for the user, and is more efficient in both on-line (up to 95 percent) and Active ECO mode (up to 98 percent). All Liebert GXT5 models are ENERGY STAR 2.0 certified, and are currently available in capacities from 500VA - 3kVA, 120 V through Vertiv channel partners in North America. Higher capacity models will be announced later this year.

Along with the highest level of equipment protection available in a rack configuration, the Liebert GXT5 offers a three-year full coverage factory warranty for the UPS and battery, a leading warranty in the industry. The system also is available with the Vertiv Power Assurance Package and other service packages, to support individual customer needs.

“Businesses are increasingly deploying compute in remote locations, stretching their resources to install, monitor and maintain the infrastructure,” said Lucas Beran, principal analyst, Cloud and Data Center, for IHS Markit. “An efficient UPS with remote management and end-to-end support would help these operations to optimize personnel and IT performance.”

“There is a premium placed on computing capabilities and low latency at the edge of the network, not only in traditional IT closets, but also in retail, healthcare, financial, education and similar small IT environments,” said Ramesh Menon, vice president of small UPS at Vertiv. “With this latest addition to our UPS portfolio, Vertiv provides features that make powering equipment at the edge more convenient and the infrastructure more future-proof.”

The Liebert GXT5 UPS can be managed remotely and has individually controlled sockets for improved security and remote reset and on/off capabilities. When used together with the free TrellisTM Power Insight, users can monitor and manage up to 100 supported Vertiv devices.

The Liebert GXT5 UPS seamlessly integrates with other products in the Vertiv channel portfolio to support single-rack or more complex edge deployments. These models replace similar capacities in the Liebert GXT4 product line.

For more information on Liebert GXT5 UPS, Vertiv and the Vertiv channel program, visit Vertiv.com.

About Vertiv
Vertiv brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs around 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.       

Contact:
Vince McMorrow
T 614-383-1622
Vince.McMorrow@Fahlgren.com

 

Related Articles

Partner Login

Language & Location