The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Cross connect cabinets allow for termination of and cross-connections between cabling elements. These enclosures provide a wide array of functionalities that meet your business and budget requirements. Integrating systems such as putting DSLAM and cross connect chambers in a single enclosure reduce deployment cost and simplify transition to digital services.

These are integrated interface systems that include housings, terminal fields, and cables to provide interface between feeder and distribution cables.

Some enclosures integrate a protective, ventilated compartment for weather-hardened DSLAM electronics with a weather-sealed compartment for cross connect fields in a single enclosure. They can either be configured as aerial enclosures with a cross-connect capacity range of 200 to 900 pairs or as pad-mount types that can range from 400 to 1200 pairs.

Some units allow upgrade of active DSL network and increase the termination capability for an existing cross connect cabinet without disrupting service or circuit downtime, reducing installation expense and labor costs.

View Outdoor Enclosures Products

Related Links

xperience, Expertise, Speed: Business Qualities that Make the Difference

Hibernia Networks selected Vertiv as its partner to design and build two fully integrated cable landing stations on each side of the Atlantic Ocean based on our experience, expertise, and deployment speed. 

Harnessing IT to Secure Your Transport Network

It’s no surprise then that transportation networks (rail, air and/or sea) are now becoming more technology-defined to keep pace with passenger growth and to provide better customer experience.

Partner Login

Language & Location