Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Vertiv Partners with GRC to Offer Highly Efficient Liquid Cooling Solution for High-Density Data Centers and Edge Applications

March 29, 2021

The Vertiv™ Liebert® VIC is now available throughout Asia, Australia and New Zealand

Singapore [March 23, 2021] – Vertiv, (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Liebert® VIC, its first liquid immersion cooling solution for high density-data centers. The solution was developed in partnership with GRC (Green Revolution Cooling), the leader in single-phase immersion cooling for data centers. Available throughout Asia, Australia and New Zealand, the Liebert VIC offers improved cooling efficiencies in dense computing environments that increasingly support data-intensive applications such as the Internet of Things (IoT), edge computing and automation. 

The Liebert VIC is a single-phase immersion cooling solution that can support high-density loads of up to 100 kW per rack, utilizing warm water. It uses the ElectroSafe™ dielectric liquid coolant, an odorless, non-toxic, single-phase coolant which is both electrically and chemically inert and has 1,200 times the heat capacity of air. This higher heat capacity means that servers with high heat densities can be cooled more effectively, reducing cooling energy costs up to 95%.

“Liquid immersion cooling is increasingly becoming an attractive option for many data center and colocation facilities, as it not only supports high-compute environments but also promises improved efficiencies, sustainability and reliability compared to traditional cooling solutions,” said Dhruv Varma, vice president of Business Development, APAC at GRC.

“Demand for a wide range of compute-intensive applications, including faster streaming platforms for both video and gaming, requires even more latency-free computing power,” said Chee Hoe Ling, vice president for Infrastructure Solutions, Vertiv Asia. “With Liebert® VIC, our customers can meet their high density objectives and rely on this highly efficient thermal solution option to cost-effectively deploy high performance computing options to their customers.”

The liquid cooling technology used by Liebert VIC reduces environmental disturbances such as moisture, dust and poor air quality. In addition, use of warm water cooling enables a highly efficient and low operating cost solution. The Liebert VIC can be deployed in any location as it is less dependent on geographical climate. Its modular design enables it to be deployed quickly within weeks, minimizing the need for data center space construction or renovations.

For more information on the Liebert VIC and Vertiv’s full portfolio of thermal management solutions, visit Vertiv.com.

 

About Vertiv Holdings Co

Vertiv Holdings Co (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

CONTACT

Katrina Tirante

T +6326203600 Ext 7666

E Katrina.Tirante@vertiv.com

 

Reinier Dungca

T +6326203600 Ext 7657

E Reinier.Dungca@vertiv.com

PARTNERS
Overview
Partner Login

Language & Location