Sorry, this page isn't available for your location.

The page you're viewing is for English (ANZ) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ANZ) region.

Australian ASX 100-listed data centre operator uses Vertiv prefabricated modular infrastructure to speed Port Hedland facility build time and strengthen data centre performance in the Pilbara region

Port Hedland, Australia [December 12, 2024] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, has helped NEXTDC (ASX: NXT) unlock new digital opportunities for Australia’s Pilbara region, delivering robust power and cooling infrastructure to its Port Hedland data centre. The new deployment supports the region’s need for robust data centre support to allow local government and industry to continue digitalization growth and the adoption of AI. 

NEXTDC provides colocation and connectivity services to Australian and international organisations. The company operates 16 data centre facilities throughout the country, with another five sites currently in the planning and development stages. NEXTDC is a leader in the industry in edge computing, extending sophisticated data centre capabilities beyond major urban areas and delivering foundational digital services to remote regions. 

PH1 Port Hedland is NEXTDC’s Port Hedland data centre, located in the remote Pilbara region of Western Australia, which services the port operations of local mining, oil and gas, and Federal Government sectors. Within the facility, Vertiv’s integrated modular data centre solutions operate close to the region’s Vocus telecommunications fibre network, helping to make cloud-based services—including AI and machine learning—available to NEXTDC’s PH1 Port Hedland customers. 

“Before NEXTDC’s PH1 Port Hedland facility opened, data generated in the Pilbara often travelled 1,600 kilometres to Perth for processing. The high latency introduced by this extensive route introduced challenges for major resource organisations and other local industries,” said Adam Gardner, head of product at NEXTDC. “Innovative solutions, including those enabled by AI, frequently require low latency, reliable connectivity with real-time data access. These major Australian organisations turned to complex, bespoke point solutions to partially alleviate the digital proximity challenges, often at a significant cost to backhaul the data. 

“NEXTDC’s PH1 empowers the region’s businesses and allows them to innovate and optimise like never before. Vertiv’s strength in Edge data centre builds—particularly in far-flung locations like Port Hedland—meant they were an ideal partner for NEXTDC’s in-house expertise. The Vertiv prefabricated infrastructure solution at PH1 optimised build time and was a great fit to service the region’s operational, safety, and productivity needs,” Gardner continued. 

Vertiv designed, procured, and implemented a complete prefabricated modular, rugged data centre for Stage 1 of the facility’s total capacity. The prefabricated approach allowed NEXTDC to overcome logistical issues because of the area’s remoteness, using capital city-built pre-engineered components and on-site standardised construction processes to reduce remote assembly costs and speed time to deployment. As a scalable, modular solution, the Vertiv deployment can be rapidly expanded to support additional growth. Meanwhile, the solution’s ruggedised design is tailored to withstand the Pilbara desert’s harsh environmental conditions. 

“Standard data centre equipment isn’t usually specified for these conditions. Vertiv knew and understood this, and together, we made sure to use condensers appropriately rated at 55 degrees Celsius,” said NEXTDC project manager Mark Hamilton. “Plus, we considered the facility’s resilience in the event of a cyclone. So, PH1 Port Hedland has tie-downs to steel fixings, appropriate to withstand high wind pressures, and includes substantive protection around critical equipment to endure a flying tree, should an event occur. 

The modular solution is Tier III Uptime Institute-certified and uses refrigerant-based air cooling. It also promotes scalability, should NEXTDC introduce increasingly popular alternative liquid cooling methods. Other features include a high-efficiency UPS system, which supports the environment’s high-density power requirements, and lithium-ion batteries for longer-lasting power. 

“We’re excited to have delivered a robust facility that will offer the Pilbara region access to technologies that improve how industries operate. Mining and oil and gas are big power consumers. As AI becomes more commonplace, these businesses can draw real-time data from their site operations and use it to identify more efficient methods of extracting resources or using trucks,” said Hamilton. 

The enablement of AI-driven, real-time data processing will play an even more prominent role amid NEXTDC’s second edge data centre build in the Pilbara region. NEXTDC’s NE1 Newman facility also leveraged the strong partnership between Vertiv and NEXTDC. Located 600km from Port Hedland and near several mines, the NE1 facility is almost identical to the PH1 facility with additional Stage 1 capacity. Hamilton noted, “This approach perfectly represents the modular and flexible nature of Vertiv’s prefabricated solutions: they are ready and able to service autonomous mines and other advanced programs.” 

“NEXTDC is bringing metro-level compute modular data centres, complete with all the security, safety, low-latency, and uptime resilience that you would expect of a large data centre in a major city, to geographically dispersed and previously-isolated locations,” said Tony Gaunt, vice president of Asia at Vertiv. “Together, we’re making access to the major cloud providers the new status quo for Australia’s most prominent and founding industries and allowing local businesses to capitalise on AI technologies with high-speed connectivity.” 

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

  

CONTACT

Jacob Penfold (for Vertiv)
Jacob.penfold@watterson.com.au
+61 411 345 145

PARTNERS
Overview
Partner Login

Language & Location