Sorry, this page isn't available for your location.

The page you're viewing is for English (ANZ) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ANZ) region.

AVR vs. UPS – Which one should you get for your gaming PC?

Choosing the best power device for your needs is a real headache. With the world’s continued digitization, ensuring reliability and continuity of electrical power to your devices isn't just a convenience but an absolute need. The stakes are high, be it simply running a small home office, managing a high-powered data center, or just keeping the household running and the electronics safe from getting damaged. This dilemma often begs the question: which of these two, Automatic Voltage Regulators (AVRs) or Uninterruptible Power Supplies (UPSs), is a more efficient solution? 

Both of these devices have their own pros and cons and can be used for different requirements and scenarios. Understanding their nuances is necessary to secure your investments from the harmful and unpredictable nature of power supply.

Understanding Automatic Voltage Regulators (AVRs)

Automatic Voltage Regulators, or AVRs, from the name itself, are electronic devices designed to regulate voltage levels for your equipment or appliances. Basically, they protect the equipment from voltage fluctuations that occur mainly from the power supply. This type of regulator is needed, especially in areas with unstable electrical grids. AVRs protect sensitive equipment from voltage spikes and drops and maintain operational efficiency by minimizing energy loss during voltage regulation. Although AVRs are vital in controlling the voltage, they do not have power backup during outages, which is crucial for some equipment, so you can power them off yourself and save anything that needs saving.

AVRs are generally a more cost-effective choice than other power protection devices if your only concern is power surges that are harmful to household devices. However, you must also note that some of the AVRs in the market are not suitable for managing large power fluctuations over an extended period.

Discovering Uninterruptible Power Supplies (UPSs)

Uninterruptible Power Supplies, or UPSs, are indispensable for maintaining power to essential equipment during a power outage. They offer safe power backup from stored power in internal batteries for the attached electronic equipment. This seamless transition not only protects against data loss and hardware damage in sensitive computing environments but also actively monitors incoming power and switches to battery power instantly upon detecting a power failure. Additionally, UPSs come with surge protectors that guard your equipment against power surges and spikes.

Although UPSs are generally more expensive than simple voltage regulators, these devices actually keep your equipment running during power outages to ensure continuity enough to let you save your work or power off your devices. They also have surge protectors that guard your equipment against power surges and spikes.

Introducing the Vertiv™ UPS

Power disturbances pose a significant threat, especially to sensitive devices—they can potentially cause data loss, irreversible damage, and very costly downtime. Vertiv has taken action to combat these risks with its different UPS systems, which are equipped not only with comprehensive surge protection and power conditioning capabilities but also with power backups that can help you immensely protect your assets.

Different types of Vertiv™ UPSs in the market today aim to protect everyone's devices, especially now with the unpredictable electrical supply in most countries. Here are the three UPSs for your unique requirements:

  1. Standby UPS – this UPS provides basic protection and can switch to batteries when power fails. This type of UPS is ideal for environments where the power supply is relatively stable, and the need for continuous power conditioning is minimal.
  2. Line-interactive UPS – this is another type of UPS that can handle minor power fluctuations without switching to battery power. This type is best for small to medium-sized businesses, home offices, and environments with relatively stable power but occasional disturbances.
  3. Online UPS – this provides the highest form of protection for your devices. It always supplies power through the battery, ensuring no interruption. Its double-conversion process effectively isolates the connected equipment from common power problems like surges, sags, and spikes.

Familiarize yourself with your environmental condition and equipment's technical requirements before choosing the type of UPS you need. This understanding will ensure you make the right choice for your power protection needs.

AVR vs. UPS

Several factors must be considered when comparing AVRs to UPSs. Here are some key points to consider when choosing the right device for your requirements.

  1. Performance in Power Fluctuations. Both AVRs and UPSs are designed to manage voltage fluctuations, but aside from that, UPS can also provide crucial backup power in the event of a total power loss. AVRs are best needed in areas with unstable electricity that frequently experience surges or drops in voltage. However, UPSs are indispensable in environments where even a brief power interruption can cause data loss, equipment failure, or operational disruption. 
  2. Backup Time and Capacity. One of the most significant differences between AVRs and UPSs is their capability to provide power during outages or just keep your devices on for a time to do your business. AVRs do not have built-in power sources and merely regulate the power that passes through them. On the other hand, UPSs can store electrical energy in their built-in batteries and provide power immediately when the primary power source fails. The amount of uptime will depend on the UPS model that you will choose.
  3. Ease of installation and Maintenance. AVRs are more compact and easier to install and maintain because they don't have batteries that need to be regularly tested and maintained compared with UPSs. Depending on the model, installing a UPS might need professional help because of all the system settings that need to be configured and set for optimal performance.

The choice between an AVR and a UPS largely depends on your equipment's specific requirements and environmental considerations. Understanding these differences will help you make an informed decision aligning with your power protection needs.

Related Articles

UPS Buying Guide Image

Blog Posts

UPS Buying Guide
PARTNERS
Overview
Partner Login

Language & Location